Technical FAQs

Ask a Question

Where is the ATV61HD45N4 EMC filter connection located?

Issue:
Where is the ATV61HD45N4 EMC filter connection located?

Product Line:
ATV61, ATV71

Environment:
All

Cause:
Need to disconnect EMC filter

Resolution:
The EMC filter is located on SW101 of the Filter Board. Have to look inside the drive at bottom left.
Was this helpful?
What can we do to improve the information ?