Technical FAQs

Ask a Question

What is the mechanical interlock for (2) LC1F contactors?

Issue:
What is the mechanical interlock for (2) LC1F contactors?

Product Line:
TeSys F-Line Contactors

Environment:
All Product Lines

Cause:
Can not find it in the Digest

Resolution:
For horizontal mounting of (2) 3 or 4 pole LC1F contactors of the same rating:

(2) LC1F115  =  LA9FF970
(2) LC1F150  =  LA9FF970
(2) LC1F185  =  LA9FG970
(2) LC1F265  =  LA9FJ970
(2) LC1F330  =  LA9FJ970
(2) LC1F400  =  LA9FJ970
(2) LC1F500  =  LA9FJ970
(2) LC1F630  =  LA9FL970
 
Was this helpful?
What can we do to improve the information ?