Technical FAQs

Ask a Question

Customer is asking for a single phase 208V to 240V step-up transformer for an XW+ Inverter

There is no direct single phase 208V to 240V transformers offered by Scheider Electric.
Customer would need to choose between 208:236V and a 208:250V transformers currently offered by Schneider-Electric (Square D). These are rated for 7.5kVA at 30A.

208V:236 V = Part number 1S446F wiring diagram 4
208V:250V = Part Number 1.5S82F wiring diagram 2

Contact Square D Low Voltage Distribution for more support on the unit at 888-778-2733 Options 1 and 1.
Was this helpful?
What can we do to improve the information ?