Technical FAQs

Ask a Question

What handle kits are available for the D10 disconnect switches?

Issue:
What handle kits are available for the D10 disconnect switches?

Product Line:
D10 Disconnect Switches

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
For 30, 60, 100, and 200A rated disconnects in NEMA 1, 3, 3R, 4, and 12 enclosures:

5-6" interior depth = D11SF4
6-10" interior depth = D11SF10
10-16" interior depth = D11SF16

The handle kit includes the switch "stub shaft actuator" + extension shaft + handle & gasket + hardware
Was this helpful?
What can we do to improve the information ?