Technical FAQs

Ask a Question

Is a surface mount cover available equal to the flush mount QOC20UFWG and QOC30UFWG for use on the wide gutter riser load centers?

Issue:
Selection

Product Line:
QO Load Center

Environment:
Selection

Cause:
Surface installation

Resolution:
No, we do not offer a surface mount equivalent. However, the flush cover could be used in a surface mount installation. The cover would merely extend .60" past the enclosure on all four sides. 

Was this helpful?
What can we do to improve the information ?