Technical FAQs

Ask a Question

Is there a HOMELINE equivalent to the QO13040M200TFT load center?

Issue:
Cross reference

Product Line:
QO and Homeline Load Center

Environment:
Cross reference

Cause: 
Selection of Homeline for the feed thru application

Resolution:
No, there is not. We used to offer a close equivalent, HOM1632L200TCFT, which could be converted to a 200A main breaker. However, it has been obsoleted and is no longer available. 
Was this helpful?
What can we do to improve the information ?