Technical FAQs

Ask a Question

What operating levers are available for the L1442M limit switch?

Issue:
The L1442M does not come with an operating lever.

Product Line:
L100/L300 Cable Pull Limit Switches

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
There are 3 options to choose from depending on the length needed:

1.50" = part number KA

2.50" - part number KO

3.00" = part number KB
 
Was this helpful?
What can we do to improve the information ?