Technical FAQs

Ask a Question

Does the HKA225S4 OEM I line interior have Aluminum , or Copper bussing?

Issue:
Does the HKA225S4 OEM I line interior have Aluminum , or Copper bussing?

Product Line:
I Line OEM Interiors

Environment:
Application

Cause:
Clarification

Resolution:

The Bussing for the 400A interior is Aluminum,  2.25" in width.
Was this helpful?
What can we do to improve the information ?