Technical FAQs

Ask a Question

What is lead time on ordering an IP54 ATV61W........N4U version drive?

Issue:
What is lead time on ordering an IP54 ATV61W........N4U version drive?

Product Line:
Altivar ATV61W  IP54 or NEMA 12

Environment:
All

Cause:
What is the standard lead time to get one of these IP54 rated drives?

Resolution:
The lead time will depend on the HP size of the drive.  You can expect to have a 20 to 45 day lead time.   Please contact the CCC at 1888 778 2733 to get any lead time information.
Was this helpful?
What can we do to improve the information ?