Technical FAQs

Ask a Question

What retaining kit is required for back feeding a branch breaker in the HOM4080L225PC or HOM4080L225PRB load center?

Issue:
Application

Product Line:
Homeline

Environment:
Retaining Kit

Cause:
Accessory selection

Resolution:
If backfeeding a 125A maximum, 2 pole Homeline breaker, use HOM4RK2HA. If backfeeding a 150A - 200A, 2 pole (uses 4 spaces) Homeline breaker, use HOM5RK.

Was this helpful?
What can we do to improve the information ?