Technical FAQs

Ask a Question

What are the part numbers for the adapter to mount the ATV32 control module rotated 90 degrees?

Issue:
part number for mounting accessory

Product Line:
ATV32

Environment:
All Altivar 32 models and serial numbers

Cause:
None

Resolution:
The part numbers for the mounting accessories for the ATV32 drive is as follows:

 
Was this helpful?
What can we do to improve the information ?