Technical FAQs

Ask a Question

Do we have any information on how far the heat sink fans and DC choke will stick out the back of the enclosure when you use the flange mounting kit?

Issue:
Do we have any information  on how far the heat sink fans and DC choke will stick out the back of the enclosure when you use the flange mounting kit?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to know how far the choke and fan will stick out the back of the enclosure.

Resolution:
See the table below  The C dimensions below.

Was this helpful?
What can we do to improve the information ?