Technical FAQs

Ask a Question

What is the maximum operation altitude for an ATV61/71 drive without derating?

Issue:
What is the maximum operation altitude for an ATV61/71 drive without derating?

Product Line:
Altivar 61, Altivar 71, ATV61, ATV71

Environment:
All

Cause:
High altitude operation for ATV61 and ATV71 drives.

Resolution:
The drive can be installed up to 1000 Meter without derating.  1000 meters to 3000 meters derating the drives current by 1 % per additional 100 meters.  Limited to 2000 meters for the Corner Grounded distribution network.

Conversion
1000 meters = approximately  3280 feet

Was this helpful?
What can we do to improve the information ?