Technical FAQs

Ask a Question

What is the replacement push button cap for the ZB4BA0 extended push button heads?

Issue:
What is the replacement push button cap for the ZB4BA0 extended push button heads?

Product Line:
22mm Push Buttons & Operator Interfaces

Environment:
All Product Lines

Cause:
Can not find it in the Digest

Resolution:

White: ZBL1

Black: ZBL2

Green: ZBL3

Red: ZBL4

Yellow: ZBL5

Blue: ZBL6

6 Assorted Colors: ZBL9
Was this helpful?
What can we do to improve the information ?