Technical FAQs

Ask a Question

Can the fusible Heavy Duty Safety Switches be applied at 50 Hertz (Hz)?

Issue:
Product Features

Product Line:
Heavy Duty Safety Switches

Environment:
Voltage system

Cause:
application

Resolution:
Yes, the Fusible Heavy Duty Safety Switches can be applied at 50 Hz and this is marked on the wiring diagram of the switch, which is located on the back of the cover/door. Contact the fuse manufacturer to determine how to select fuses.
Was this helpful?
What can we do to improve the information ?