Technical FAQs

Ask a Question

What is the recommended tightening torque for the mounting bolts on a 9422A1 and 9422A2 handles?

Issue:
What is the recommended tightening torque for the mounting bolts on a 9422A1, and 9422A2 handles?

Product Line:
9422 Handle Mechanisms

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
Tightening torque for the two handle mounting bolts is 60 to 72 In/lbs.
Was this helpful?
What can we do to improve the information ?