Technical FAQs

Ask a Question

What is form Q8 on a 9013 pressure switch?

Product line:
9013 pressure switches 

Resolution: 
It is for a plastic Flange.  ( 120 F max. temp. and 80 psi maximum pressure) on Class 9013 FSG, FYG.  Available on 1/4" NPSF Internal thread only.

 

Was this helpful?
What can we do to improve the information ?