Technical FAQs

Ask a Question

Is the D325NR suitable for use as service equipment?

Issue:
Application

Product Line:
General Duty Safety Switch

Environment:
Service Entrance

Cause:
Validation

Resolution:
Yes, the D325NR is suitable for use as service equipment. Confirmation will be noted on the switch wiring diagram. The neutral must be bonded to the enclosure with the green neutral bonding screw that is provided with the switch.

Was this helpful?
What can we do to improve the information ?