Technical FAQs

Ask a Question

Does Square D by Schneider Electric offer a QMB twin 60amp/30amp rated branch switch?

Issue:
Does Schneider Electric offer a QMB323TW, 3 pole 240V switch with a 60/30 unit amperage rating?

Product Line:
QMB panelboard, switchboard with QMB distribution.

Environment:
Switch ampere rating

Cause:
Application

Resolution:
Yes, Square D offers a 60amp/30amp twin branch switch. The catalog number is QMB362T21W, This is a 3pole, 600Vac Maximum, 60 A/30 A Twin that requires 6 inches of mounting space.
 

Was this helpful?
What can we do to improve the information ?