Technical FAQs

Ask a Question

What is the torque spec on the lug connection to the bus for an MAL361000 ?

Issue:
Lug torque tightening

Product Line:
Molded Case Breakers

Environment:
MAL, MHL

Cause:
Installation

Resolution:

 

 
 
 
180# in. for lug mounting screw
Was this helpful?
What can we do to improve the information ?