Technical FAQs

Ask a Question

Are 9050JCK relays polarity sensitive for DC coil?

Issue:
Are 9050JCK relays polarity sensitive for DC coil?

Product Line:
9050JCK timing relays - GIC Product

Environment:
US Product

Cause:
This is an important factor when applying relay and frequent cause for troubleshooting

Resolution:
Ye, the coils on these relays are polarity sensitive.  Positive must always be on terminal 2.  Wiring diagrams are included on the instruction sheet which is attached.
 
Was this helpful?
What can we do to improve the information ?