Technical FAQs

Ask a Question

What jumpers are available for NSYTRV42?

Issue:
Trying clarify the jumper options for the NSYTRP24D terminal block.

Product Line:
Linergy TR Screw terminal blocks.

Environment:
Linergy TR NSYTRV42,NSYTRV42BL, NSYTRAV42AR,NSYTRAV42RD,NSYTRAV42GN,NSYTRAV42WH,NSYTRAV42BK,,

Cause:
To clarify all of the jumpers available for the NSYTRV42 TERMINAL BLOCKS.

Resolution:
All of the jumpers for this terminal block is found on page 20 in the LINERGY CATALOG 9080CT1301.
 Red Jumpers: NSYTRAL42 is a 2 pole jumper, NSYTRAL43 is a 3 pole jumper, NSYTRAL44 is a 4 pole jumper,  NSYTRAL45 is a 5 pole jumper, NSYTRAL410 is a 10 pole jumper, NSYTRAL420 is a 20 pole jumper.
Blue Jumper 10 pole is NSYTRAL410BL and Green 10 pole jumper is NSYTRAL410GN
Was this helpful?
What can we do to improve the information ?