Technical FAQs

Ask a Question

What is the SCCR rating for 9422 type T disconnects

ISSUE
SCCR rating for 9422TEF10

PRODUCT LINE
Class 9422 Flange mount, fusible DIsconnect

ENVIRONMENT
The 9422 T Series Disconnect Switch Assemblies

CAUSE:  
Customer's need to know SCCR for application

RESOLUTION
These Switch assemblies when mounted in a correctly sized enclosure and per UL
requirements are suitable for use on a Circuit capable of delivering not more than 10,000 rms
symmetrical amperes at 600 V maximum when protected by Class H or Class K fuses or a
maximum of 100,000 rms symmetrical amperes at 600 V maximum when protected by Class J,
or Class R fuses.

KEYWORDS: 9422TEF10 9422TCF30, 9422TCF33, 9422TDF60, 9422TDF63, 9422TF2 9422TG2, 9422TF3

 
Was this helpful?
What can we do to improve the information ?