Technical FAQs

Ask a Question

What is the difference between the SC2040M200F and the replacement SC2040M200PF Combination Service Entrance Devices?

Design Features

Product Line:
Combination Service Entrance Devices

Product Design

Replacement unit

The SC2040M200F is the old design that has been replaced by the new Plug-On Neutral(PoN) Design, catalog number SC2040M200PF. The basic concept of these CSED devices are the same, the main difference is the load center interior, which now accepts the Plug-On Neutral Arc Fault and Ground Fault breakers, that do not contain the white 'pigtail' connection.
Was this helpful?
What can we do to improve the information ?