Technical FAQs

Ask a Question

Are ClimaSys CU Cooling Units thermoelectric or fluid/gas systems?

Issue:
Are ClimaSys CU Cooling Units thermoelectric or fluid/gas systems?

Product Line:
ClimaSys Enclosure Accessories - GIC Product

Environment:
US Product

Cause:
The type of cooling method can be an important design criteria

Resolution:
The ClimaSys systems use R134a (HFC).  This is a gas that respects the ozone.
 
Was this helpful?
What can we do to improve the information ?