Technical FAQs

Ask a Question

Replacing 9007B54NC2

Issue:
What replaces the 9007B54NC2?

Product Line:
9007C Limit Switches - GIC Product

Environment:
US Product

Cause:
These limit switches are still in use in certain applications

Resolution:
The 9007B54NC2 was a gravity actuated limit switch.  There is no direct replacement for this switch.  The 9007C54N2 is the closest product as it is a light torque actuation (25oz-in), but it is not gravity actuated.
 
Was this helpful?
What can we do to improve the information ?