Technical FAQs

Ask a Question

Where can I find information about the ATV32 drives frame sizes?

Issue:
Where can I find information about the ATV32 drives frame sizes?

Product Line:
Altivar 32 or  ATV32 family

Environment:
All

Cause:
They are confused about the ATV32 frame sizes some show letters and some show letter and numbers.

Resolution:
See the attached document:
Frame size S1 and A are the same frame sizes
Frame size S2 and B are the same frame sizes
Frame size S4 and C are the same frame sizes
Frame size S5 and D are the same frame sizes


 
Was this helpful?
What can we do to improve the information ?