Technical FAQs

Ask a Question

Are the disconnect handles on the E-flex enclosed products Lock Out/Tag Out compatible?

Issue:
Are the disconnect handles on the E-flex enclosed products Lock Out/Tag Out compatible?

Product line:
Class 8839, Type EFD, E-flex enclosed drive systems.

Environment:
All models, All serial numbers.

Cause:
Clarification of product features needed.

Resolution:
Yes.  All E-flex cabinets have a factory installed disconnect handle that contains Lock Out / Tag Out compatible features.
Was this helpful?
What can we do to improve the information ?