Technical FAQs

Ask a Question

How do I install or migrate Powerlink PCS software on a Windows 7 operating system?

Issue:
How do I install or migrate Powerlink PCS software on a Windows 7 operating system?
What is the difference between PCS and LCS?
How do I upgrade PCS software?

Product Line:
Powerlink G3 Lighting Control Panelboard

Environment:
Commercial Building Lighting Control, North America

Cause:
The customer is attempting installation of PCS software on Windows 7 or other unsupported operating system.   PCS was replaced by LCS software in 2007.   PCS software is not supported on Microsoft Windows operating systems that have been released after 2007.  

Resolution:
One needs to purchase and install either LCSBASIC or LCSADVANCED.  Owners or PCS are eligible to purchase "upgrade" packages of LCS for a discounted rate by showing evidence that they already own a license of PCS.



PCS101
Was this helpful?
What can we do to improve the information ?