Technical FAQs

Ask a Question

What are the short circuit ratings for the Vario switches

Issue:
What are the short circuit ratings for the Vario switches

Product Line:
Vario Motor Control Switches - GIC Product

Environment:
US Product

Cause:
SCCR ratings are important for certain applications

Resolution:
The SCCR rating for the vario line will depend on the upstream protection means and these are not UL98 rated. See attached document for SCCR ratings.
 
Was this helpful?
What can we do to improve the information ?