Technical FAQs

Ask a Question

Bracket for Snap Switch on a 9002AW11

Issue:
What is the part number for the bracket that holds the snap switch on a 9002AW11?

Product Line:
9002 Foot Switches - GIC Product

Environment:
US Product

Cause:
This part is not listed in current literature

Resolution:
The bracket is part number 2502-D3-X1.  This part is only for the 9002AW11
 
Was this helpful?
What can we do to improve the information ?