Technical FAQs

Ask a Question

Where can I find the location of the conduit connection on the ATV61 or ATV71 Plus drives?

Issue:
Where can I find the location of the conduit connection on the ATV61 or ATV71 Plus drives?

Product Line:
Altivar ATV61 and ATV71 plus drives only

Environment:
All

Cause:
Confused about where the conduit entry is on the ATV61/ATV71 Plus Drives

Resolution:
You can find the conduit dimensions location in instruction bulletin 30072-454-96 starting on page 21.
 

Example: 




 

Was this helpful?
What can we do to improve the information ?