Technical FAQs

Ask a Question

What is the retaining kit for use with the HOM4080L225PGC, Series S04, load center to retain a back fed branch circuit breaker?

Issue:
Selection

Product Line:
Homeline

Environment:
Retaining kit

Cause:
Accessory selection

Resolution:
If the retaining kit is for use with a 125 ampere, or less, branch breaker use HOM4RK2HA. If for use with a 150 - 200 ampere branch breaker, use HOM5RK.
Was this helpful?
What can we do to improve the information ?