Technical FAQs

Ask a Question

2 Position 22mm Selector Switch Contact Actuation

What is the actuation of contacts on a two-position 22mm switch?

Product Line:
22mm Push Buttons - GIC Product

US Product

Different switches actuate contacts in different ways

The actuation of contacts depends on three things; wiring, mounting position, type of contact.  For a 22mm switch, the actuation is relatively simple.  when any of the two-position switches are turned to the right, the switch actuates all of the contacts which are mounted to it.  The attached chart shows this actuation graphically.
Was this helpful?
What can we do to improve the information ?