Technical FAQs

Ask a Question

Determining trip type on GV2 manual motor starter

Issue:
Is it possible to determine the type of trip on a GV2 manual starter without using a signalling contact block?

Product Line:
GV2 Manual Motor Starters

Environment:
US Product

Cause:
It may be desirable to determine this without a signalling contact block.

Resolution:
The type of trip cannot be determined without a signalling contact block.
Was this helpful?
What can we do to improve the information ?