Technical FAQs

Ask a Question

What is the serial number prefix for the Altivar drives that are made in India?

Issue:
What is the serial number prefix for the Altivar drives that are made in India?

Product Line:
Altivar Drives

Environment:
All

Cause:
The drives serial number starts with JM1448 and no one can ID this serial number.

Resolution:
The drives that are made in India will have a serial number that starts with JM1448. 
Was this helpful?
What can we do to improve the information ?