Technical FAQs

Ask a Question

Which microswitch is inside the 9002AW118?

Issue:
Which microswitch is inside the 9002AW118?

Product Line:
9002 Foot Switches - GIC Product

Environment:
US Product

Cause:
This swtch may need to be replaced

Resolution:
The 9007CO3S6 is the microswitch within the 9002AW118.  Additional parts can be found on the attached bulletin. 
**Note** This is an older bulletin and should only be used to reference the 9002AW118 foot switch.  For all other foot switches, use the newer bulletin 65013-010-31
Was this helpful?
What can we do to improve the information ?