Technical FAQs

Ask a Question

Legends for 9001K type Flush Plates

Issue:
Which legend types are compatible with the 9001K Flush Plates

Product Line:
9001K 30mm Pushbuttons - GIC Product

Environment:
US Product

Cause:
Correct legend sizing is necessary for certain applications

Resolution:
The 9001KN1 series of legend plate will be the only size which will fit correctly.
Was this helpful?
What can we do to improve the information ?