Technical FAQs

Ask a Question

What are the specifications and acceptable wire size ranges for use with the RXZ type sockets?

Issue:
What are the specifications and acceptable wire size ranges for use with the RXZ type sockets?

Product Line:
RXM Relay - GIC Product

Environment:
US Product

Cause:
Wire size and other characteristics are important design criteria

Resolution:
The specifications and characteristics of the RXM relays is attached.  Wire size is specified on the third page.
 
Was this helpful?
What can we do to improve the information ?