Technical FAQs

Ask a Question

Is a remote reset option available for a short circuit trip on the U-Line motor starters?

Issue:
Is a remote reset option available for a short circuit trip on the U-Line motor starters?

Product Line:
TeSys U-Line Manual Motor Starters

Environment:
All Product Lines

Cause:
Can not find it in the Digest

Resolution:
No. The handle must physically be switched to the Off position, and then to the On position to clear the trip.
Was this helpful?
What can we do to improve the information ?