Technical FAQs

Ask a Question

What splits are offered on a factory assembled 225a main lugs split-bus NQ panel ?

 
 
Issue:
Split bus circuit configurations
Product Line:
Panelboards
 
Environment:
NQ
 
Cause:
Panel offer
 
Resolution:
 
 

We can offer an 18/30, 30/18 or 30/30 circuit split . All would fit in a 44"h can.
 
Was this helpful?
What can we do to improve the information ?