Technical FAQs

Ask a Question

What is the resistance on NEMA size 5, series B, AC coils?

Issue:
What is the resistance on NEMA size 5, series B, AC coils?

Product Line:
NEMA AC Magnetic Coils

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
The resistance on these electronic coils cannot be measured with an Ohmmeter. A properly functioning coil, when isolated from it's control circuit, will draw between 0.3 mA and 10 mA (depending on the coil voltage rating) when connected to a 9V battery (polarity unimportant).


 

Was this helpful?
What can we do to improve the information ?