Technical FAQs

Ask a Question

What is the resistance on NEMA size 5, series A, AC coils?

Issue:
What is the resistance on NEMA size 5, series A, AC coils?

Product Line:
NEMA Magnetic AC Coils

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
At 20 degrees C operating temperature (60 Hz only):

120V = 0.95 Ohms

208V = 2.67 Ohms

240V = 3.83 Ohms

277V = 5.49 Ohms

347V = 7.15 Ohms

380V = 9.84 Ohms

480V = 15.5 Ohms

600V = 24.6 Ohms
Was this helpful?
What can we do to improve the information ?