Technical FAQs

Ask a Question

What is the resistance on NEMA size 4 AC coils?

Issue:
What is the resistance on NEMA size 4 AC coils?

Product Line:
NEMA Magnetic AC Coils

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
At 20 degrees C operating temperature (60 Hz only):

120V = 3.57 Ohms

208V = 10 Ohms

240V = 14.5 Ohms

277V = 20.8 Ohms

380V = 36.4 Ohms

480V = 58.2 Ohms

600V = 92.4 Ohms
Was this helpful?
What can we do to improve the information ?