Technical FAQs

Ask a Question

What is the resistance on NEMA size 2, 3 & 4 pole, AC coils?

Issue:
What is the resistance on NEMA size 2, 3 & 4 pole, AC coils?

Product Line:
NEMA Magnetic AC Coils

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
At 20 degrees C operating temperature (60 Hz only):

24V = 0.48 Ohms

120V = 12.1 Ohms

208V = 43.7 Ohms

240V = 48.4 Ohms

277V = 71.5 Ohms

380V = 122 Ohms

480V = 239 Ohms

600V = 376 Ohms
Was this helpful?
What can we do to improve the information ?