Technical FAQs

Ask a Question

What is the resistance on NEMA size 2 AC coils?

Issue:
What is the resistance on NEMA size 2 AC coils?

Product Line:
NEMA Magnetic AC Coils

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
At 20 degrees C operating temperature (60 Hz only):

24V = 0.7 Ohms

120V = 17.8 Ohms

208V = 60 Ohms

240V = 71 Ohms

277V = 104 Ohms

380V = 178 Ohms

480V = 274 Ohms

600V = 800 Ohms
Was this helpful?
What can we do to improve the information ?