Technical FAQs

Ask a Question

What does the suffix 25K indicate on an MPZ device?

Issue:
What does the suffix 25K indicate on an MPZ device?

Product Line:
Mini power zone

Environment:
MPZ mini power zone

Cause:
Product features

Resolution:
The 25K suffix indicates the MPZ is rated at 25KAIC. The standard AIC is 18K. The 25K units have a higher rated 25K AIC primary main breaker installed, and so the entire unit AIC is then rated at 25K. Same for the 65K.

Was this helpful?
What can we do to improve the information ?