Technical FAQs

Ask a Question

What does the DGS6 represent in part number 9001KP38DGS6G31?

Issue:
What does the  DGS6 represent in part number 9001KP38DGS6G31?

Product Line:
Control Relays

Enviroment:
IEC  Control

Cause:
DGS6 means

Resolution:

It indicates a 135V DC light module which is used in switchgear.
Was this helpful?
What can we do to improve the information ?