Technical FAQs

Ask a Question

Will the motor phase rotation change if I swap two of the line supply wires going to the variable frequency drive?

Issue:
Will the motor phase rotation change if I swap two of the line supply wires going to the variable frequency drive?

Product Line:
Altivar drives

Environment:
All models and serial numbers

Cause:
None

Resolution:
No, the phase rotation will not change if any of the line supply wires are changed.  Swapping two of the output motor wires UVW or T1 T2 T3 will cause the motor phase rotation to change.

 
Was this helpful?
What can we do to improve the information ?