Technical FAQs

Ask a Question

What covers are available for the QO154M200PG load center?

Issue:
Selection

Product Line:
QO Load Center

Environment:
Selection

Cause:
Cover selection

Resolution:
The only cover offered for the QO154M200PG is QOC54UF, which is a flush mount cover. It could also be used for a surface mount installation bu the cover would extend .60" past the four sides of the enclosure.

Was this helpful?
What can we do to improve the information ?